Skip to main content
Associate II
March 13, 2025
Solved

Cube AI doesnt generate all files needed

  • March 13, 2025
  • 2 replies
  • 988 views

I am working with the Nucleo-N6 Board and i am trying to get a neural network to run on the ART accelerator. The following steps are done to create the project:

  • Make new project
    • Select NUCLEO-N657X0-Q in the Board Selector
    • In Project Structure select "Secure domain only" and "Appli"
    • Then "Finish" and "Generate demonstration code"
  • Configure .ioc
    • Middleware and Software Packs: X-Cube-AI 10.0.0 for context "Application" and check box under core and select "System performance" under Application
    • Configure LPUART1 Mode: Asynchronous
    • Then again select X-Cube-AI under Middleware and Software Packs and add own network (TFLite) and use LPUART1 under "Platform Settings" (b.t.w. some weird windows pop up which say "Please wait, configuring platform settings" which cant be closed)
    • Resolve Errors in RCC and Clock Configuration
  • Save .ioc and generate Code

While building -> fatal error in "app_x-cube-ai.c" where the line #include "aiSystemPerformance.h" cant be resolved.
Are my steps to create a project with AI correct?

STM32CubeIDE Version: 1.17.0
OS: Ubuntu 22.04.5 LTS
X-Cube-ai: 10.0.0
N6 Firmware: 1.0.0

Best answer by fauvarque.daniel

You can find the online documentation here 

https://stedgeai-dc.st.com/assets/embedded-docs/index.html

with a chapter on how to perform inferences on the target.

AI Code generation with MX for N6 has been fixed in the upcoming April release. At this point the systemPerformance application is not supported (it should be removed from the possible choices), you can use the Template Application for a simple template.

You'll still have to manage the loading of the secure and non secure programs from the FSBL code. This part is not directly generated by X-CUBE-AI but can be generated with MX.

I recommend using the latest STM32CubeMX 6.14 as some bug fix have been done also on N6 support

Regards

Daniel

 

2 replies

Julian E.
Technical Moderator
March 18, 2025

Hello @LukasOst ,

 

Sorry for the late answer.

We have some bug when regenerating code with CubeMX and X Cube AI and we think your issue may come from that.

I've ask the dev team for help. I'll update you when I have more information.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Explorer
March 19, 2025

Hello Julian.

Will a simple guidance of NPU be published and in the next update? I use NUCLEO-N6 Board too and can't wait to run my own model on N6 chips.

Really looking forward for your reply.

Best wishes,

fauvarque.daniel
fauvarque.danielBest answer
ST Employee
March 21, 2025

You can find the online documentation here 

https://stedgeai-dc.st.com/assets/embedded-docs/index.html

with a chapter on how to perform inferences on the target.

AI Code generation with MX for N6 has been fixed in the upcoming April release. At this point the systemPerformance application is not supported (it should be removed from the possible choices), you can use the Template Application for a simple template.

You'll still have to manage the loading of the secure and non secure programs from the FSBL code. This part is not directly generated by X-CUBE-AI but can be generated with MX.

I recommend using the latest STM32CubeMX 6.14 as some bug fix have been done also on N6 support

Regards

Daniel

 

LukasOstAuthor
Associate II
March 24, 2025

Hey @fauvarque.daniel thanks for your answer.

My problem at the moment is that the number of choices in CubeMX when creating a new project is a bit overwhelming. Can you maybe explain when do i need to use the FSBL? From the information i found i understood it that way that i need FSBL if i want to store the Network in extern memory. Is this correct?

Also i am kind of confused by the architecture of the project after creating a new project in CubeMX/CubeIDE. Why is it setup like a "nested" project?