Skip to main content
Associate III
February 19, 2025
Solved

Deploying deep learning model on nucleo-H753ZI Validation on target error

  • February 19, 2025
  • 1 reply
  • 571 views

Screenshot 2025-02-19 224520.png

 It is fine until validation on desktop... But when it comes to validation on target, the above shown error is displaying...
Can anyone please help me with this error... I am trying this since 3 months...

Best answer by Julian E.

Hello @Pinagadi_Meghana ,

 

Indeed, you need to enable to enable the "Automatic compilation and download" to flash the validation firmware in the N6 for the validation on target to work. 

In my case, I am using STM32CubeIDE:

JulianE_0-1740055525507.png

 

Thank you very much @ahsrabrifat for your help!

 

Have a good day,

Juian

1 reply

Senior III
February 19, 2025
Julian E.
Julian E.Best answer
Technical Moderator
February 20, 2025

Hello @Pinagadi_Meghana ,

 

Indeed, you need to enable to enable the "Automatic compilation and download" to flash the validation firmware in the N6 for the validation on target to work. 

In my case, I am using STM32CubeIDE:

JulianE_0-1740055525507.png

 

Thank you very much @ahsrabrifat for your help!

 

Have a good day,

Juian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
February 20, 2025

What are the options that i need to give at communication port, TX pin and RX pin...
when i selected them  by looking at the pinout configuration, it is saying that no board is connected...???
i will share the screenshot of it please have a look