Gain setting for microphones on STWINKT1B
Hi guys
I have a couple of questions.
I've been using the microphones on STWINKT1B to record some events for about a month now. I've utilized both the FP-SNS-DATALOG1 and FP-SNS-DATALOG2 firmware for data logging. While the digital mic (imp34dt05) delivers a good signal, there have been instances where the analog mic (imp23absu) produces noisy output with high-pitched tones, either intermittently or throughout the recording. I'm not sure why this is happening, but the interference has certainly compromised the quality of the recording. If anyone's interested, I have attached a recording for review. I'm curious if anyone has any insights into why this might be occurring.
My other question relates to the gain settings for these microphones. Is there a way to adjust the gain of the microphone? According to the datasheet of the imp23absu, the output feeds into an op-amp. Is the gain adjustable, or is it fixed?
Additionally, according to the JSON configuration file of FP-SNS-DATALOG2, the sensitivity is set to 3.0517578125e-05. What does this value mean? It seems highly specific. Is it the output voltage at 94 dB-SPL (@ 1 kHz)? Can I modify this setting?
I realize this is a lengthy inquiry, but I really appreciate any insight you can offer. Thank you in advance.