Getting errors with STM32Cube AI Studio
- February 20, 2026
- 4 replies
- 351 views
Dear all,
With the new STM32Cube AI Studio tool, I am getting the following errors (see attached log file). I am using it with the kit STM32N6570-DK.
I tried the same model as in the tutorial (https://www.youtube.com/watch?v=3zyIpB5o9zQ). I am getting the same type of error with other models as well.
Thank you for your help. I am looking forward to being able to use this new tool.
-------------------------------------------------------------------------------------------------------------------------------------------------
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Validation/Src/ai_wrapper_ATON.c:386:10: warning: suggest parentheses around assignment used as truth value [-Wparentheses]
386 | while (aton_buf = npu_get_input_buffers_info(instance, nn_info->n_inputs))
| ^~~~~~~~
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Validation/Src/ai_wrapper_ATON.c:393:10: warning: suggest parentheses around assignment used as truth value [-Wparentheses]
393 | while (aton_buf = npu_get_output_buffers_info(instance, nn_info->n_outputs))
| ^~~~~~~~
In file included from C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_profiler.c:27:
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_profiler.c: In function 'LL_ATON_LIB_ConvInteger':
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_profiler.c:206:31: warning: format '%d' expects argument of type 'int', but argument 4 has type 'int32_t' {aka 'long int'} [-Wformat=]
206 | LL_ATON_PROFILER_PRINTF("%s k=%d %d scale=%g\n", conv_name, k, maxmax_k, kern->scale[k]);
| ^~~~~~~~~~~~~~~~~~~~~~~ ~~~~~~~~
| |
| int32_t {aka long int}
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_util.h:43:46: note: in definition of macro 'LL_ATON_PROFILER_PRINTF'
43 | #define LL_ATON_PROFILER_PRINTF(...) printf(__VA_ARGS__)
| ^~~~~~~~~~~
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_profiler.c:206:41: note: format string is defined here
206 | LL_ATON_PROFILER_PRINTF("%s k=%d %d scale=%g\n", conv_name, k, maxmax_k, kern->scale[k]);
| ~^
| |
| int
| %ld
C:/Users/papam/.stm32cubeaistudio/workspace/demo_face_detection/.ai/run/run-1/Middlewares/ST/AI/Npu/ll_aton_profiler.c:282:33: warning: format '%d' expects argument of type 'int', but argument 4 has type 'int32_t' {aka 'long int'} [-Wformat=]
282 | LL_ATON_PROFILER_FPRINTF(f, "%s %d\n", conv_name, maxmax); // log((float)maxmax) / log(2.0));
| ^~~~~~~~~ ~~~~~~
| |
| int32_t {aka long int}