HardFault error in ai_platform_network_process()
Hello,
I have implemented https://wiki.st.com/stm32mcu/wiki/AI:How_to_perform_motion_sensing_on_STM32L4_IoTnode this project. When I run the program I had a hard fault error when function enters ai_platform_network_process(). I have incremented the heap and stack sizes. I don't know what else I can do to run properly. As below, after ai_network_run() it enters ai_platform_network_process(). This function is source coded and cannot see the content of this function.
If you can help me, I will be very grateful...
Regards.
static void AI_Run(float *pIn, float *pOut)
{
ai_i32 batch;
ai_error err;
/* Update IO handlers with the data payload */
ai_input[0].data = AI_HANDLE_PTR(pIn);
ai_output[0].data = AI_HANDLE_PTR(pOut);
batch = ai_network_run(network, ai_input, ai_output);
if (batch != 1) {
err = ai_network_get_error(network);
printf("AI ai_network_run error - type=%d code=%d\r\n", err.type, err.code);
Error_Handler();
}
}