How to set input data in application template using CubeMx.Ai
In the project, the input data of keras model is a 2-d vector consisted of float x1 and float x2. But in the cubemx.ai generated application template code, the data type is ai_u8 as follows:
ai_u8 *in_data = NULL;
ai_u8 *out_data = NULL;
Then ,I modified it as follows :
ai_float *in_data = NULL;
ai_float *out_data = NULL;
in_data[0]=0.1;
in_data[1]=-0.1;
But it will got errors as follows while ai_run(in_data, out_data) executed.
TEMPLATE -Error (ai_network_run) -type=0x12 code=0x17
Then How to set input data in application template, and where can I got the codes details of the error, I look forward to your reply.Thanks a lot!