How to train a convolutional neural network with data collected by ADC?
Dear ST Engineer,
I have downloaded the AER audio recognition AI app from Github. There are about 50 kinds of audio in the app for training convolutional neural network (CNN). If I need to train a specific audio that I have customized, what should I do?For example, I collected a frame of 20ms data with 48K sampling rate and stored it in array X[960], with 960 data points in total. How do I use this array X to train convolutional neural network (CNN)?In addition, where is the interface function after the trained model is compiled into the project by CUBE.AI?