Question
How to use the generate code with the IA resources ApplicationTemplate
Hello,
I have some questions about using the code generator
I am currently using an STM32F446 and I want to use a Keras model driven by python to make a prediction on the data retrieved by the micro-controller in order to get better results.
- I found on internet that I should use X-CUBE-AI version 3.4 with ApplicationTemplate as a resource. Is it really the right resource, if I want to do only the prediction on the micro-controller ?
- If yes, I have, once the code is generated, an MX_X_X_CUBE_AI_Process function that seems empty, do I have to complete it or does it work as it ? If I have to complete it, is it possible to indicate me how to complete it and especially with what.
void MX_X_CUBE_AI_Init(void)
{
MX_UARTx_Init();
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
}
void MX_X_CUBE_AI_Process(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
}- Where is called the function to retrieve the data from the micro-controller and transform it ? With this, the data can be used by the program to make the prediction from the Keras model?
- Last question, Where is the function to retrieve the result of my prediction. In which form is the results ?
If someone have more information about how to use the generator code it could be really helpful for me.
thanks