HSDPython_SDK missing in DATALOG2_3.0.0
So I downloaded the new datalog2 demo zip file (early 2025)
Installed the bin file into my STWINBOX using STM32programmer and verified that file was the same as target
I believe this version is a bit more stable at connecting to the iphone app ST_BLE_Sensor 5.2.4, using BLE.
However
* I managed to easily lock the stwinbox by pressing the [START] arrow button on the app's Sensors page. the middle green LED stopped blinking and was stuck in either on or off and comms was lost.
* The python lib was not present in the zip archive. I started the hsdatalog_GUI.py in datalog 2.3 instead and it had trouble connecting over usb. After connecting, it locked up on a "loading templates" window,. Here's the debug log:
2025-03-26 13:18:39,745 - HSDatalogApp.st_hsdatalog.HSD_link.HSDLink - INFO - Trying to open communication using libhs_datalog_v2...
2025-03-26 13:18:39,748 - HSDatalogApp.st_hsdatalog.HSD_link.communication.PnPL_HSD.hsd_dll - INFO - Platform Architecture: 64bit
HSD_DLLv2: libusb_close!
HSD_DLLv2: libusb_close!
HSD_DLLv2: libusb_close!
HSD_DLLv2: libusb_close!
HSD_DLLv2: libusb_close!
HSD_DLLv2: libusb_close!
HSD_DLLv2: CONNECTED!
2025-03-26 13:18:40,202 - HSDatalogApp.st_hsdatalog.HSD_link.communication.PnPL_HSD.PnPLHSD_com_manager - INFO - Communication Engine UP (libhs_datalog_v2 DLL/so) (PnPLHSD_com_manager.py:45)
2025-03-26 13:18:40,203 - HSDatalogApp.st_hsdatalog.HSD_link.HSDLink_v2 - INFO - Vespucci PnPL Commands (HSDLink_v2.py:89)
2025-03-26 13:18:40,203 - HSDatalogApp.st_hsdatalog.HSD_link.communication.STWIN_HSD.STWINHSD_com_manager - INFO - Communication Engine DOWN (libhs_datalog_v1 DLL/so) (STWINHSD_com_manager.py:142)
2025-03-26 13:18:40,204 - HSDatalogApp.st_hsdatalog.HSD_link.HSDLink - INFO - Commmunication Opened correctly
Traceback (most recent call last):
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_dtdl_gui\Widgets\ConnectionWidget.py", line 123, in clicked_COM_connect_button
self.controller.load_device_template(board_id,fw_id)
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_hsdatalog\HSD_GUI\HSD_Controller.py", line 339, in load_device_template
super().load_local_device_template(dev_template_json)
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_dtdl_gui\STDTDL_Controller.py", line 106, in load_local_device_template
self.components_dtdl = self.__dt_manager.get_components()
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File "C:\Users\A508196\AppData\Local\Packages\PythonSoftwareFoundation.Python.3.12_qbz5n2kfra8p0\LocalCache\local-packages\Python312\site-packages\st_pnpl\DTDL\device_template_manager.py", line 56, in get_components
for content in self.get_root_component().contents:
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
AttributeError: 'NoneType' object has no attribute 'contents'
Traceback (most recent call last):
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_dtdl_gui\STDTDL_MainWindow.py", line 196, in s_device_connected
for i in reversed(range(self.widget_device_config.layout().count())):
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
AttributeError: 'NoneType' object has no attribute 'layout'
Traceback (most recent call last):
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_dtdl_gui\Widgets\ConnectionWidget.py", line 123, in clicked_COM_connect_button
self.controller.load_device_template(board_id,fw_id)
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_hsdatalog\HSD_GUI\HSD_Controller.py", line 339, in load_device_template
super().load_local_device_template(dev_template_json)
File "c:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples\st_dtdl_gui\STDTDL_Controller.py", line 106, in load_local_device_template
self.components_dtdl = self.__dt_manager.get_components()
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File "C:\Users\A508196\AppData\Local\Packages\PythonSoftwareFoundation.Python.3.12_qbz5n2kfra8p0\LocalCache\local-packages\Python312\site-packages\st_pnpl\DTDL\device_template_manager.py", line 56, in get_components
for content in self.get_root_component().contents:
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
AttributeError: 'NoneType' object has no attribute 'contents'
PS C:\ST\STM32CubeFunctionPack_DATALOG2_V2.3.0\Utilities\HSDPython_SDK\examples>