implement multi-model scheduling with FreeRTOS using STM32Cube.AI ?
Hi all,
I’m currently working on an Edge AI project using the NUCLEO-N657X0-q and I've run into a roadblock regarding multi-model deployment.
I need to run 2 or 3 models on this MCU, scheduled via FreeRTOS. While I can get a single model working fine with STM32Cube.AI Studio, I’m struggling to find a detailed workflow for managing multiple instances.
Specific questions:
API Naming: How to properly configure Cube.AI to generate unique prefixes for multiple models to avoid link-time conflicts?
Memory/Buffer Sharing: Is there a standard way to share a single activation buffer between models to save RAM, given they are called sequentially via FreeRTOS?
Task Scheduling: Any known issues or best practices for calling stai_network_run() within a FreeRTOS task? (e.g. stack size or re-entrancy).
I’ve checked the ST Edge AI Core docs but couldn't find a concrete example for this multi-model + RTOS use case. If anyone has a reference project or can point me to the right Application Note, I’d really appreciate it.
Thanks!