Skip to main content
FKara.3
Associate III
September 2, 2023
Solved

lsm6dsv16x_sensor_fusion.c compliaton error in ESP32 hardware

  • September 2, 2023
  • 1 reply
  • 1387 views

Hello, 

 

I try to write the sensor_fusion.code in ESP32. I get below compilation error;

Compilation error: 'LSM6DSV16X_SFLP_GYROSCOPE_BIAS_TAG' was not declared in this scope

 

here is my code;


#include <Arduino.h>
#include "lsm6dsv16x_reg.h"
#include "lsm6dsv16x_fsm_sflp_asc.h"
// #include "lsm6dsv16x_reg.c"
#include <Wire.h>


/** I2C Device Address 8 bit format  if SA0=0 -> D5 if SA0=1 -> D7 **/
#define LSM6DSV16X_I2C_ADD_L 213
#define LSM6DSV16X_I2C_ADD_H 215


/* Private macro -------------------------------------------------------------*/
/*
 * Select FIFO samples watermark, max value is 512
 * in FIFO are stored acc, gyro and timestamp samples
 */
#define BOOT_TIME         10
#define FIFO_WATERMARK    32

/* Private variables ---------------------------------------------------------*/
static uint8_t whoamI;

/* Private variables ---------------------------------------------------------*/
static lsm6dsv16x_fifo_sflp_raw_t fifo_sflp;

/* Extern variables ----------------------------------------------------------*/

/* Private functions ---------------------------------------------------------*/

static int32_t platform_write(void *handle, uint8_t reg, const uint8_t *bufp,
                              uint16_t len);

static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,
                             uint16_t len);

static uint32_t npy_halfbits_to_floatbits(uint16_t h) {
    uint16_t h_exp, h_sig;
    uint32_t f_sgn, f_exp, f_sig;

    h_exp = (h & 0x7c00u);
    f_sgn = ((uint32_t)h & 0x8000u) << 16;
   
    switch (h_exp) {
        case 0x0000u: /* 0 or subnormal */
            h_sig = (h & 0x03ffu);
            /* Signed zero */
            if (h_sig == 0) {
                return f_sgn;
            }
            /* Subnormal */
            h_sig <<= 1;
            while ((h_sig & 0x0400u) == 0) {
                h_sig <<= 1;
                h_exp++;
            }
            f_exp = ((uint32_t)(127 - 15 - h_exp)) << 23;
            f_sig = ((uint32_t)(h_sig & 0x03ffu)) << 13;
            return f_sgn + f_exp + f_sig;
           
        case 0x7c00u: /* inf or NaN */
            /* All-ones exponent and a copy of the significand */
            return f_sgn + 0x7f800000u + (((uint32_t)(h & 0x03ffu)) << 13);
           
        default: /* normalized */
            /* Just need to adjust the exponent and shift */
            return f_sgn + (((uint32_t)(h & 0x7fffu) + 0x1c000u) << 13);
    }
}

float npy_half_to_float(uint16_t h) {
    union { float ret; uint32_t retbits; } conv;
    conv.retbits = npy_halfbits_to_floatbits(h);
    return conv.ret;
}

static void sflp2q(float quat[4], uint16_t sflp[3])
{
  float sumsq = 0;

  quat[0] = npy_half_to_float(sflp[0]);
  quat[1] = npy_half_to_float(sflp[1]);
  quat[2] = npy_half_to_float(sflp[2]);

  for (uint8_t i = 0; i < 3; i++)
    sumsq += quat[i] * quat[i];

  if (sumsq > 1.0f) {
    float n = sqrtf(sumsq);
    quat[0] /= n;
    quat[1] /= n;
    quat[2] /= n;
    sumsq = 1.0f;
  }

  quat[3] = sqrtf(1.0f - sumsq);
}

void lsm6dsv16x_sensor_fusion() {
  lsm6dsv16x_fifo_status_t fifo_status;
  stmdev_ctx_t dev_ctx;
  lsm6dsv16x_reset_t rst;
  lsm6dsv16x_sflp_gbias_t gbias;

  // Initialize sensor driver interface
  dev_ctx.write_reg = platform_write;
  dev_ctx.read_reg = platform_read;
 


  // Initialize platform (if necessary)
  // platform_init();

  delay(BOOT_TIME); // Arduino delay function

  // Check device ID
  lsm6dsv16x_device_id_get(&dev_ctx, &whoamI);

  if (whoamI != LSM6DSV16X_ID) {
    while (1) {
      Serial.println("Incorrect device ID");
      delay(1000);
    }
  }

  // ... [rest of your initialization code]

  while (1) {
    uint16_t num = 0;

    lsm6dsv16x_fifo_status_get(&dev_ctx, &fifo_status);

    if (fifo_status.fifo_th == 1) {
      num = fifo_status.fifo_level;

      Serial.print("-- FIFO num ");
      Serial.println(num);

      while (num--) {
        lsm6dsv16x_fifo_out_raw_t f_data;
        int16_t *axis;
        float quat[4];
        float gravity_mg[3];
        float gbias_mdps[3];

        // ... [rest of your data handling code]

        switch (f_data.tag) {
   
        case LSM6DSV16X_SFLP_GYROSCOPE_BIAS_TAG:
          axis = (int16_t *)&f_data.data[0];
          gbias_mdps[0] = lsm6dsv16x_from_fs125_to_mdps(axis[0]);
          // ... [rest of the case]
          Serial.print("GBIAS [mdps]: ");
          Serial.print(gbias_mdps[0]);
          Serial.print("\t");
          // ... [rest of the printing]
          break;
        // ... [rest of the switch-case]
        }

      }
      Serial.println("------");
    }
  }
}



void setup() {
  // put your setup code here, to run once:
  lsm6dsv16x_sensor_fusion();  // Call the sensor fusion function

}

void loop() {
  // put your main code here, to run repeatedly:

}



int32_t platform_write(void *handle, uint8_t reg, const uint8_t *bufp, uint16_t len) {
  Wire.beginTransmission(LSM6DSV16X_I2C_ADD_L); // Assume LSM6DSV16X_I2C_ADD_L is the I2C address
  Wire.write(reg);
  for(uint16_t i = 0; i < len; i++) {
    Wire.write(bufp[i]);
  }
  return Wire.endTransmission();
}



int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp, uint16_t len) {
  Wire.beginTransmission(LSM6DSV16X_I2C_ADD_L);  // Assume LSM6DSV16X_I2C_ADD_L is the I2C address
  Wire.write(reg);
  Wire.endTransmission(false);  // Use a repeated start, so we don't release the bus

  uint16_t bytesRead = Wire.requestFrom(LSM6DSV16X_I2C_ADD_L, len);  // Request bytes from slave device
 
  for(uint16_t i = 0; i < bytesRead; i++) {
    bufp[i] = Wire.read();
  }
  return bytesRead == len ? 0 : -1;  // Return 0 if success, else -1
}


This topic has been closed for replies.
Best answer by Issamos

Hello @FKara.3 

I think that the problem is that LSM6DSV16X_SFLP_GYROSCOPE_BIAS_TAG is not defined anywhere in the code. I suggest you to properly define it. Taking a look to the exemples in this library may be helpful also.

Hope this is helpful for you. If your question is answered please check this answer as best answer to be diffused.

Best regards.

II

1 reply

Issamos
IssamosBest answer
Lead III
September 2, 2023

Hello @FKara.3 

I think that the problem is that LSM6DSV16X_SFLP_GYROSCOPE_BIAS_TAG is not defined anywhere in the code. I suggest you to properly define it. Taking a look to the exemples in this library may be helpful also.

Hope this is helpful for you. If your question is answered please check this answer as best answer to be diffused.

Best regards.

II

FKara.3
FKara.3Author
Associate III
September 26, 2023

Thank you for your response, @Issamos ;

It is not defined in sensor_fusion example in the library. How can we define it?

 

Regards,

Fehmi