n6-dk hard fault with unresponsive debugger
I have been playing with the n6-dk for a while and today something unexpected happened.
When I try to run the stock code provided in the model zoo services, the board flashes for a moment at startup and the debugger and the board become unresponsive (requiring power cycling).
Another weird thing is that if I flash the code and connect the board to a power source the code seems to be running correctly. I tried with another desktop experiencing the same issue. I also tried to do a mass erase and fresh flashing of fsbl, source, and network code.
This was not a problem before, for weeks I run the code with the board connected to my desktop, I have never seen the code crash like that (normally, if something in the code is wrong, I hit a fault and the board get stuck in a sig handler loop).
Has anyone experienced anything similar?