Skip to main content
Associate
February 10, 2025
Question

Nanoedge AI Benchmark issue

  • February 10, 2025
  • 2 replies
  • 700 views

Hi, 

im having issues with NEAI Studio. I was able to craete a project, add signals but when running the benchmark I get an error message that benchmarking was not successfull. In the log I see a lot of  this error messages:

optimizer ERROR T20* - An error occurred in neai lib due to Error in qualif, return code: 53

Regards 

Max

2 replies

Julian E.
Technical Moderator
February 10, 2025

Hello @The_Maxx ,

 

Can you attach the logs as a zip files, please?

 

Are you using the 4.6.0? Did you installed this version directly or did you do an update from a previous version?

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
The_MaxxAuthor
Associate
February 10, 2025

Hi Julian,

I installed v4.6.0 directly. No previous version.

Logs are attached.

 

BR

Max

 

Julian E.
Technical Moderator
February 10, 2025

Hello @The_Maxx ,

 

Thanks for the information.

This issue means that the search algorithm is looking outside the possible space of possibilities for the parameters of models.

We have already encountered this issue in the past and it was supposed to be fixed. But in our case, it was not really blocking. What do you mean when you say you get an unsuccessful benchmark? 

Does the benchmark stop? Do you have anything is the "Validation Step"? 

 

Is it possible for you to share your project? It not, no worries.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Roger SHIVELY
ST Employee
February 10, 2025

Hello @The_Maxx 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Roger