Skip to main content
Sandrine
Associate
March 15, 2022
Solved

NanoEdge AI library usage on different devices

  • March 15, 2022
  • 1 reply
  • 820 views

 Is it needed to do the learning on every device? Or can the library be used on all devices of the same class?

This topic has been closed for replies.
Best answer by Sandrine

It is possible to use the same library (both static and dynamic) on all devices of the same class. The following scenario is possible: prepare representative HW/SW setup then learn the dynamic model (Anomaly Detection), backup the knowledge and clone the knowledge to every device (working under similar conditions), please see :

 https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_anomaly_detection_(AD)#Backing_up_and_restoring_the_library_knowledge

1 reply

Sandrine
SandrineAuthorBest answer
Associate
March 15, 2022

It is possible to use the same library (both static and dynamic) on all devices of the same class. The following scenario is possible: prepare representative HW/SW setup then learn the dynamic model (Anomaly Detection), backup the knowledge and clone the knowledge to every device (working under similar conditions), please see :

 https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_anomaly_detection_(AD)#Backing_up_and_restoring_the_library_knowledge