Skip to main content
DmitryR
Associate III
March 15, 2025
Question

Neural-ART Accelerator (NPU) component for ST Edge AI Core does not install

  • March 15, 2025
  • 2 replies
  • 845 views

Good day, 

 

preparing to an online workshop I am trying to install prerequisites. However the component en.stedgeai-stneuralart-10.0.0.zip does not install, STM32CibeIDE says: "This file is either corrupted or not a recognized package.".

 

Regards,

Dmitry

2 replies

Julian E.
Technical Moderator
March 17, 2025

Hello @DmitryR ,

 

You are installing X Cube AI (and npu) with the integrated CubeMX in CubeIDE?

 

Make sure to use STM32CubeIDE v1.17.0 minimum.

Then you can try to eitheir uninstall X Cube AI v10.0.0 and then install it again in STM32CubeMX

Or uninstall X Cube AI v10, install the st edge ai core as standalone (where you downloaded the stneuralart) and install X Cube AI after that, as he will use the standalone st edge ai core.

 

Have a good day,

Julian

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DmitryR
DmitryRAuthor
Associate III
March 26, 2025

Hi @Julian E. ,

 

do you mean that the X-Cube-AI v. 10.0.0 is the same as en.stedgeai-stneuralart-10.0.0.zip download?

 

Regards,

Dmitry

hamitiya
ST Employee
March 26, 2025

Hello,

The zip file en.stedgeai-stneuralart-10.0.0.zip is a component that you will need to install directly from X-CUBE-AI. You need first to install X-CUBE-AI 10.0.0, and once you open a board with ST Neural-ART Accelerator (such as STM32N6570-DK) you will be asked to install ST Neural-ART package if not available. You will enter your zip when asked.

How to install X-CUBE-AI:

AI:How to install X-CUBE-AI through STM32CubeMX - stm32mcu

If you select STM32N6570-DK instead of NUCLEO like the documentation, you will have a pop-up asking for en.stedgeai-stneuralart-10.0.0.zip

Hope its clearer

 

Best regards,

Yanis

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.