Skip to main content
JZhou.6
Associate II
July 21, 2022
Question

Neural network engineering built with CubeAI 7.10, and then initialized in MDK5 to error(type=33)

  • July 21, 2022
  • 5 replies
  • 2203 views

I built the LSTM network with keras 2.6.0 and generated the MDK project with CubeAI 7.10. However, in running the program AIInit() reported an error with an error type of 33.Do you know what the problem is? Thank you very much!0693W00000QLmlBQAT.png

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
July 22, 2022

Doesn't the documentation of that function tell you what error codes it can return, and why?

Also try a 'Go To Definition' on AI_ERROR_NONE - there you should also find the definitions of other error codes ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JZhou.6
JZhou.6Author
Associate II
July 22, 2022

I looked at the meaning of the error type. This is (AI_ERROR_CREATE_FAILED), but there is no documentation telling me how to solve this problem. I wouldn't have this problem with CubeAI 6.0.If you know where to help documentation or workarounds, please let me know. Thank you very much!0693W00000QLsnhQAD.png

Andrew Neil
Super User
July 22, 2022

so now you can look at the source of that function, and see where that code is returned.

that'll tell you what it was trying to create; should also show why it failed.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JZhou.6
JZhou.6Author
Associate II
July 22, 2022

I've been using GO TO define refe's method to locate the error. But when it comes to this API, it appears undefine.0693W00000QLsuiQAD.png

Andrew Neil
Super User
July 22, 2022

Try stepping into it, then.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JZhou.6
JZhou.6Author
Associate II
July 22, 2022

0693W00000QLt4JQAT.png0693W00000QLt44QAD.pngI can't get into this function. But I found that the value of the (AI_NETWORK_DATA_CONFIG) parameter generated by CubeAI7.1 is NULL. This is also the input parameter of this function. Could it be a problem here. Do you have a reference document for reporting errors, thank you!

Andrew Neil
Super User
July 22, 2022

@JZhou.6​ "I can't get into this function"

How do you mean?

Are you sure that's the one returning the error?

"Do you have a reference document"

Here?

0693W00000QLtGtQAL.png

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JZhou.6
JZhou.6Author
Associate II
July 22, 2022

Thank you�?I have also checked a lot of documents, and I have not seen the error analysis.