Skip to main content
Associate III
October 21, 2025
Solved

porting yolov11(best_saved_model/best_integer_quant.tflite) model to stm32mp257,

  • October 21, 2025
  • 1 reply
  • 236 views

hi,all.

 I used “best_saved_model/best_integer_quant.tflite” to perform inference on the PC,it's looks success!

tflite_model = YOLO("/home/alientek/best_saved_model/best_integer_quant.tflite")

# Run inference
results = tflite_model("/home/alientek/hander1_1.jpg")

 

and output like this.

(yolov11) alientek@ubuntu:~/yolov11$ python test1.py 
/home/alientek/.conda/envs/yolov11/lib/python3.10/site-packages/requests/__init__.py:86: RequestsDependencyWarning: Unable to find acceptable character detection dependency (chardet or charset_normalizer).
 warnings.warn(
WARNING ⚠️ Unable to automatically guess model task, assuming 'task=detect'. Explicitly define task for your model, i.e. 'task=detect', 'segment', 'classify','pose' or 'obb'.
Loading /home/alientek/best_saved_model/best_integer_quant.tflite for TensorFlow Lite inference...
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.

image 1/1 /home/alientek/hander1_1.jpg: 640x640 1 handler1, 1760.9ms
Speed: 38.9ms preprocess, 1760.9ms inference, 26.5ms postprocess per image at shape (1, 3, 640, 640)

 

But when I deploy to the stm32mp257 using the following code, the target is not detected.

for (int w = 0; w < 8400; w++)
{
 float cx = data[0 * 8400 + w];
 float cy = data[1 * 8400 + w];
 float w_box = data[2 * 8400 + w];
 float h_box = data[3 * 8400 + w];

 // Find class with max probability
 float max_score = 0;
 int max_class = -1;
 for (int c = 0; c < num_classes; c++)
 {
 float score = data[(4 + c) * 8400 + w];
 if (score > max_score)
 {
 max_score = score;
 max_class = c;
 }
 }

 if (max_score > confidence_threshold)
 {
 ObjDetect_Results det;
 det.x = cx;
 det.y = cy;
 det.w = w_box;
 det.h = h_box;
 det.class_id = max_class;
 det.confidence = max_score;
 detections.push_back(det);
 }
}

 

Best answer by Julian E.

Hi @fanronghua0123456,

 

I think this question is part of this thread. Please don't duplicate threads.

Re: porting yolov11 model to stm32mp257. - Page 2 - STMicroelectronics Community

 

Have a good day,
Julian

1 reply

Julian E.
Julian E.Best answer
Technical Moderator
October 27, 2025

Hi @fanronghua0123456,

 

I think this question is part of this thread. Please don't duplicate threads.

Re: porting yolov11 model to stm32mp257. - Page 2 - STMicroelectronics Community

 

Have a good day,
Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.