Problem when moving a github project model to stm32cube AI
First , the github project is this
https://github.com/Xiaobin-Rong/gtcrn/tree/main
It has converted to onnx and tensorRT for ppl to use
but when i load the onnx model into stm32 for optimize/import (setting , compression : none , optimization : balance)
it just jumps out an error
X-cube-AI version is 9.1.0
ST Edge AI Core v1.0.0-19894
INTERNAL ERROR: Trying to remove node_339 which has multiple inputs
is it because the multi input and output network limitation or something else?
and if i success to import this model
how to deal with the multi dimensional tensor arrays that the github author demo ?
if you want to test on the model
there is the link for the onnx and tensorRT model
https://github.com/Xiaobin-Rong/TRT-SE/tree/main/online/models
Thanks in advance
Uveuvenouve