Solved
Resource Management Error: Building ResNet8 TFLite model on Nucleo-N657X0-Q (X-CUBE-AI)
- February 19, 2026
- 1 reply
- 202 views
Hi,
I am a beginner working with the STM32 Nucleo-N657X0-Q and trying to deploy a pre-trained model from the ST Model Zoo.
Environment:
- Board: Nucleo-N657X0-Q
- Tools: STM32CubeMX (latest), STM32CubeIDE (latest), X-CUBE-AI (latest)
- Model: resnet8_32_tfs_int8.tflite
- Workflow: Followed the STM32CubeIDE 2.0.0 workflow tutorial from the ST Community. (STM32CubeIDE 2.0.0 workflow tutorial - STMicroelectronics Community)
Configurations:
- Heap Size: 0x4000
- Stack Size: 0x2000
- Toolchain/IDE:STM32CubeIDE
- Used default X-CUBE-AI settings for code generation.
The Issue:
After generating the C code in CubeMX and attempting to build the project in STM32CubeIDE, the build fails with the following error
After generating the C code in CubeMX and attempting to build the project in STM32CubeIDE, the build fails with the following error
Steps Taken:
- Imported the TFLite model into the X-CUBE-AI simplified GUI.
- Verified the model successfully (Analysis report shows it should fit).
- Generated the code and opened the project in STM32CubeIDE.
- Attempted to build.
Could someone guide me on whether my Heap/Stack allocations are insufficient for the model, or if there are additional linker script adjustments/additional configuration change needed for the N6 series?
Attached are the screenshots of my Cube MX configuration and the console error output. Any help would be greatly appreciated