Skip to main content
Associate
February 5, 2026
Question

ST Edge AI Core v3.0: GTCRN, LiSenNet: "Incomplete symbolic shape inference"

  • February 5, 2026
  • 1 reply
  • 224 views

Hi everyone,

I’m currently working with the STM32N6 and the new ST Edge AI Core v3.0, trying to deploy some Speech Enhancement models. I’m specifically targeting architectures like LiSenNet, GTCRN, and UL-UNAS because they are theoretically designed for embedded hardware..

However, the workflow with STM-model-zoo-services is giving me a hard time:

  1. Analyze Failure: After training -->best_model.onnx --> stedgeai.exe analyze -m best_model.onnx --> fails immediately.

  2. Quantization Issues: When I try to quantize, I consistently get an "Incomplete symbolic shape inference" error. It seems the compiler struggles with dynamic shapes or specific operators even though these models should be compatible.

Is the ST Edge AI Core v3.0 limited to simpler architectures like TCN for Speech Enhancement, or is there a way to make GTCRN work?

1 reply

Julian E.
Technical Moderator
March 6, 2026

Hi @giuug,

 

The Stedge AI core is indeed limited for now regarding speech enhancement.

Even TCN, improving support for such architecture is one of the main focus for the next release (v4.1).

 

So GTCRN is not supported at the moment.

 

We are aware of the shortcomings regarding timeseries architectures support. We are working on it.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.