Skip to main content
Associate
July 10, 2023
Question

STEVAL-MKI227KA WHO_AM_I Register Value does not match

  • July 10, 2023
  • 14 replies
  • 5469 views

I am trying to use Unico 9.14.6.0 to get the evaluation module to work for the LSM6DSV16X.
But I am getting an error that says it's an unexpected device based on the WHO_AM_I register.

  • STEVAL-MKI109V3 updated to v3.48.3
  • STEVAL-MKI227KA (Labeled STEVAL-MKI227AA on board)

    I have switched the jumpers to the SDx SCx but that didn't seem to work either. 
    Tried both mac and windows.

    SCR-20230710-mlqq.png

    Any help would be appreciated
This topic has been closed for replies.

14 replies

niccolò
ST Employee
July 11, 2023

Hi @JeffWelder ,
Welcome to ST community =D

the issue you encountered is really strange,
could you check if it works with other adapters?
also, can you share a picture of the setup?

Niccolò

Associate
July 11, 2023

Hi Niccolò,

I only have this adapter unfortunately.
I probed the SCx and SDx lines and don't see any activity on this brand new dev kit. The lines just go high when you click connect, and low when you close the error.
Edit: Upon moving the jumpers back to QV, I see some activity, but still get the same WHO_AM_I error. 
Attached is an image of both.

Wondering if there's anything I can try.
PXL_20230711_151539423.jpgSCR-20230711-kmfp.png

Associate
July 12, 2023

It looks like the chip is being wrongfully configured.

It tries to put it into 3-wire SPI, which appears successful, but doesn't read or write correct values, failing the WHO_AM_I register test.

If I hotplug the adapter board after this configuration, I can successfully see the response of 0x70 on the WHO_AM_I register on a logic analyzer, but the GUI sees this as 0xFF since it is expecting a 3-wire SPI response.

WHO_AM_I.png

 



Associate
July 13, 2023

@niccolò 
In leiu of a software solution, if you could help me find a download link for the Unico version used in the demo webinar (Anyone can build smarter applications with this intelligent IMU), it would be greatly appreciated.

GUI Version: 9.14.0.0
Firmware Version V3.47.1e

Thanks,
Jeff

niccolò
ST Employee
July 13, 2023

Hi @JeffWelder ,

the older versions of Unico are not available to me, but I asked a colleague that works with UNICO for help, I'll get in touch as soon as he replies.

I'm not able to spot anything wrong with what you are doing, the only thing I could suggest is to uninstall and reinstall Unico on pc and reflash the board with its firmware, if you havn't already tried it.

Niccolò

Associate
July 17, 2023

@niccolò 
Any update from your colleague?

I have the STEVAL-MKI227KA working wired into my custom hardware, but want to test the advanced features using the GUI.

Federica Bossi
Technical Moderator
July 17, 2023

Hi @JeffWelder ,

We used also an older version of Unico and a Mac pc but we didn't have any problem.

Do you have a STEVAL of another product to see if it works? If not, can you try to replicate the test using another PC?

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
July 17, 2023

Hi @Federica Bossi,
I have tried to use Unico 9.14.6 on both Windows and Mac with no success.

I just saw Unico version 9.15.0 was released for Windows, so I downloaded the ProfiMEMSToolV3.53.3_00_08000000.bin to the dev-kit through STM32CubeProgrammer in DFU mode, then tried to connect to the device on my windows machine. I still get Error WHO_AM_I register does not match on both computers.

I don't have another STEVAL board of this form-factor to try, but I can guarantee the STEVAL-MKI227KA hat attached works via testing with my hardware. Happy to try any more suggestions.

For funsies, I tried a stm32nucleo with a x-nucleo-iks02a1 hat, with the STEVAL-MKI227KA plugged in, but that didn't recognize the motherboard.

Federica Bossi
Technical Moderator
July 20, 2023

Hi @JeffWelder ,

Can you give me more details about hardware and software you used for this test: For funsies, I tried a stm32nucleo with a x-nucleo-iks02a1 hat, with the STEVAL-MKI227KA plugged in, but that didn't recognize the motherboard.

Thanks

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
July 20, 2023

@Federica Bossi 
I think that test is irrelevant since I tried to load the steval-mki109v3 binary onto a nucleo-f401re board.

I am still just trying to get the GUI to work with the normal dev-kit. I can't get past the WHO_AM_I register check. Can you confirm that this configuration works with Unico?
steval-mki109v3
steval-mki227ka

Trying to get to the bottom of this I have been issuing commands using a serial terminal.

failed_who_am_i.png

The who_am_i register is not being read correctly. If you then hotplug the MEMS board, so it is no-longer in 3-wire SPI, it returns the correct 0x70 on regular SPI as shown on my logic analyzer image in a previous post above, but the GUI returns 00h still because it is anticipating 3-wire SPI.

If you could confirm the GUI works with the latest unico + binary, plus try these serial commands, it could help me figure out if there's a hardware issue.

Thanks,
Jeff

Associate
July 24, 2023

@Federica Bossi 
Were you or a colleague able to try any of these experiments?