STEVAL-STWINBX1 datalogger board - add digital input for logging to SD card (to sync multiple DAQs)
I am using the STEVAL-STWINBX1 development board and have downloaded the FP-SNS-DATALOG2 software to the board.
Is it possible to add another channel, in this case a digital input that will be logged to the SD card ?
I need to synchronize the data logs from different DAQ systems including the STEVAL-STWINBX1
I was thinking if the STEVAL-STWINBX1 could log a GPS PPS (Pulse Per Second) digital signal, then I could manually (offline) sync its log with the logs from the other DAQ systems.
Or is there some other technique I can use to synchronize all these logs from different DAQ systems (e.g. IRIG, NTP, EtherCAT, PTP).