Skip to main content
Yiming_Katsura
Associate
May 27, 2022
Question

STM32H735g-dk, "validate on target" step's error.

  • May 27, 2022
  • 0 replies
  • 532 views

Hi, it seems to be a common error in STM32 devices. It happens when I try to validate on target after analyze the model. I tried to fix it according to the answers in community. But those solutions given in community or other websites doesn't help. At least for my board they doesn't help.0693W00000Nqn06QAB.png 

Infomation:  

The device: STM32H735G-DK 

MCU: STM32H735IGK6 

CubeMX 6.5.0 with X Cube AI v7.1.0, v7.0.0 & v 6.0.0 

Model: The model given in official tutorial of X-cube-ai. 

  

CN15 STLK √ 

JP7: CHGR/USBFS 

SW1: Set to 1 

USART3 Enabled: PD8 & PD9 

Baud Rate: 115200 

Word Length:8 bit 

No Parity 

Stop bits: 1 

  

ST-Link connectivity works normally. (Able to connect with CubeProgrammer). 

It can be built in Keil and could be load to the board, with LD6 blinking in red and green. I am looking forward to solutions to this problem. 

Thanks 

This topic has been closed for replies.