STM32MPU25 object detection model failing to run python scripts
Hi
I am using STM32MPU25 to evaluate object detection, when i use stai_mpu_object_detection binary to run default ssd_mobilenet_v2 models , i can see object detection works.
when i run python scripts to launch application( example : launch_bin_object_detection_testdata.sh) i see below error.
root@stm32mp25-discounknownunknown:/usr/local/x-linux-ai/object-detection# sh launch_python_object_detection.sh
stai_mpu wrapper used :
machine used = stm32mp2x with GPU/NPU
user : weston
-sh: /usr/local/x-linux-ai/object-detection/stai_mpu_object_detection.py: Permission denied
i assume it may be due to weston user and root user.
so i copied all objection detection samples to /home/weston and gave appropriate permissions and change user to weston and launch application, i see below errors.
^^^^^^^^^^^^^^^^^^^^^
File "/home/weston/test/Application/ssd_mobilenet_pp.py", line 129, in get_results
return locations, classes, scores
^^^^^^^^^
UnboundLocalError: cannot access local variable 'locations' where it is not associated with a value
Traceback (most recent call last):
File "/home/weston/test//Application/object_detection.py", line 336, in new_sample
self.app.nn_result_locations, self.app.nn_result_classes, self.app.nn_result_scores = self.nn.get_results()
^^^^^^^^^^^^^^^^^^^^^
File "/home/weston/test/Application/ssd_mobilenet_pp.py", line 129, in get_results
return locations, classes, scores
can you point to environment where i can evaluate object detection models ( i followed procedure at https://github.com/STMicroelectronics/stm32ai-modelzoo-services/tree/main/object_detection to create object detection model with custom data set and deploy into stm32mpu25)
Thanks