stm32n6 gfx+cubeAI
When using stm32n6 and enabling both GFX and AI models, the runtime continuously reports errors:
"Epoch controller error interrupt: EC_IRQ = 0x00000008 Epoch controller opcode counter: 0x00000000 Epoch controller tag: 0x00000000 ATON_STD_IRQHandler()@851: irqs=0xlx Assertion '0' failed: file 'E:/TouchGFXProjects/AR_Glasses/Middlewares/AI_Runtime/Npu/ll_aton/ll_aton_runtime.c', line 855, function: __LL_ATON_RT_IrqErr"
What could be the possible cause of this? Is it related to the XSPI2 bus? both GFX and cubeAI utilize XSP2.
The model used is the official demo program: st_yolo_x_nano_480_1.0_0.25_3_st_int8.tflite from STM32N6-GettingStarted-ObjectDetection-main.
I sincerely hope that st can help me solve this problem. Thanks