Skip to main content
Will_Robertson
Associate III
September 27, 2025
Question

STM32N657 μC and STM32MP257 μP - ST Image Sensors

  • September 27, 2025
  • 0 replies
  • 400 views

Hi Chris @Chris_Young_ST, Giuseppe @gpagano, Emmanuel @Emmanuel_C and Kunliang @Kunliang_YAO

Are there plans to offer ST image sensors together with the STM32MP257F-DK and STM32N6570-D development boards as an alternative to the Sony image sensor in the B-CAMS-IMX board?

ST has an enormously strong strategic position through its global leadership in producing both image sensors and processors. This will allow ST customers to achieve unparalleled speed, efficiency and sustainability together with rapid route to market in demanding power-sensitive and low-latency machine vision and EdgeAi applications.


Our focus is on developing technologies for conservation of Europe's most beautiful and endangered dormouse, squirrel and bat species. The combination of ultra-low-power Edge AI capabilities in the STM32N657 μC and the advanced RGB-IR capabilities in ST image sensors is as exciting here as it is in the most demanding commercial machine vision applications:

https://new-homes-for-old-friends.cairnwater.com/quick-summary-new-homes-for-old-friends-belgium/

I think ST image sensor S-Boards should be able to connect directly to the STM32MP257F-DK and STM32N6570-D while ST image sensor promodules would connect to via the ST P-Board.

Will