Skip to main content
Associate
April 9, 2025
Question

Unsupported Layers Update for Segment-Anything Models

  • April 9, 2025
  • 2 replies
  • 464 views

We are aiming to deploy one of the more well-known CV models on an MCU, the segment-anything model by Facebook, but there are layers that are unsupported, and we can't exactly modify layers as it would greatly affect performance. Fortunately, time is not a concern for us in inference so the speed of the hardware is not a major challenge (as opposed to a GPU).

Is there some timeline or plan, or some way we can implement these layers ourselves internally?

LayerNormalization, MatMulInteger, DynamicQuantizeLinear, OneHot, ConvInteger, and Range

2 replies

Julian E.
Technical Moderator
April 10, 2025

Hello @junaidsiddiqui,

 

Sadly, it seems very complicated to do something here... It is too early to use your model I think with the ST Edge AI Core.

 

First, more and more layers are added as the stedgeai core is updated but I can't tell you the order or priority of which they are treated.

 

You can find the list of ONNX supported layers here:https://stedgeai-dc.st.com/assets/embedded-docs/supported_ops_onnx.html

 

It is maybe possible to replace the unsupported layers by equivalent operation using other supported layers. I am not sure that this is really possible. For example, for MatMulInteger, we support MatMul but only for float32 or QLinearMatMul but I don't know if it is the same.

 

It is probably a lot of work, and it will for sure have impact on the accuracy of the model..

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
April 10, 2025

Hi Julian,

Thanks a bunch!

I've used alternative layer operations for other AI architectures I customized on my own which I can tolerate some model accuracy.

I'll try to investigate other avenues if the case is as you put it. Appreciate all your help, Thanks!