Using images for input to ST Model zoo models
I am using the object detection code from ST model zoo.
I have a small image of 4X4 example:
const uint8_t myImage[NN_HEIGHT] [ NN_WIDTH]= {
// Row 0 (all black)
{ 255, 0, 0, 0},
// Row 1 (black, then white dot, then black)
{ 0, 255, 255, 0}, // Pixels 1 and 2 are white (center of a 2x2 dot)
// Row 2 (black, then white dot, then black)
{0, 255, 255, 0},// Pixels 1 and 2 are white
// Row 3 (all black)
{0, 0, 0, 0}
};
I want to see the output as number of dots.
I dont use the camera or display unit of the N6-DK board and I am using memcpy to load the image to the input buffer(nn_in)
The image is also loading into the input buffer as when I put a bp at the memcpy line and see nn_in its first value is shown as 255 'y'
but when I see the output which is stored in pp_output the number of objects detected are 0.
Why do i see that value??
Is using memcpy to load images to input buffer correct?
If not, why and how can I adopt another workflow?
Is there an issue with my image input??
Thanks in advance!