What the validation command does during its runtime?
- July 10, 2025
- 4 replies
- 866 views
Hi,
With the new 2.2 STEdgeAI update I have done some neural network model validations on the CM55 of the nucleo-n657x0-q board. I have also used the STLink-v3pwr to measure the power consumption while validating. What I wonder is if there is some detailed explanation on what the validation command does during its runtime, more specifically what happens on the target board.
Attached is a .stpm of a example validation using my custom model with 10 data samples, as can be seen 10 spikes are recorded with some activity between them. How can this activity be classified? Is a inference the time from the start of a spike until the next spike, or is a inference only the spike and the time between them is some other activity?
Thanks in advance,
Brian.