X-CUBE-AI: error while analyzing model
Hi,
I have followed the tutorial https://www.youtube.com/watch?v=grgNXdkmzzQ&t=4s to test X-CUBE-AI with CubeMX5.0.1, but the step 'Analysis' just end with an error message without any details. I have received the same error with CubeIDE which comes with integrated CubeMX.
If I try to run 'Analysis' of the same model after selecting the board I receive the error as shown below. Could anyone please help me in figuring out where could be the problem? Do I require to install Python to run X-Cube-AI? That is not mentioned in the users manual or tutorial.
Thank you in advance!
Achyut
The error:
--------------
Analyzing model
Neural Network Tools for STM32 v1.1.0 (AI tools v4.1.0)
TOOL ERROR: Traceback (most recent call last):
File "site-packages\tensorflow\python\pywrap_tensorflow_internal.py", line 18, in swig_import_helper
File "imp.py", line 296, in find_module
ImportError: No module named '_pywrap_tensorflow_internal'
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "site-packages\tensorflow\python\pywrap_tensorflow.py", line 58, in <module>
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 631, in exec_module
File "site-packages\tensorflow\python\pywrap_tensorflow_internal.py", line 28, in <module>
File "site-packages\tensorflow\python\pywrap_tensorflow_internal.py", line 20, in swig_import_helper
File "c:\python35\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 714, in load_module
ImportError: DLL load failed with error code -1073741795
Failed to load the native TensorFlow runtime.
See https://www.tensorflow.org/install/errors
for some common reasons and solutions. Include the entire stack trace
above this error message when asking for help.