Skip to main content
pignaz
Visitor II
August 29, 2023
Question

X-CUBE-AI: Mismatch in presence of batch size

  • August 29, 2023
  • 0 replies
  • 3261 views

Hello,
I'm using X-CUBE-AI to implement an ONNX model on a STM32H757I board.
In particular, the ONNX model is a PyTorch model that has been exported using the onnx library offered by the pyTorch framework.

The analysis procedure fails and reports the following error message:

INTERNAL ERROR: Mismatch in presence of batch size: [['H: 40', 'W: 1', 'CH: 6'], (Empty)] vs. [['BATCH: 1', 'CH: 6']]

But the model input have static dimension, and running get_inputs() on the onnx model returns:

NodeArg(name='actual_input_1', type='tensor(float)', shape=[40,1,6])

The model seems to comply with the constraints reported in the STM32CubeAI documentation.  

Can you help me identifying what's wrong with the model?

Thank you!
Andrea

This topic has been closed for replies.