Skip to main content
Visitor II
July 24, 2023
Question

X-CUBE-AI, tflite LSTM model: Unsupported layer types

  • July 24, 2023
  • 3 replies
  • 3915 views

Hi,

I’m currently trying to upload the following LSTM model into a STM32L476RG via X-CUBE-AI

CFrancesco_0-1690184731832.png

Uploading the Keras .h5 model works well, however when I try to upload the TensorFlow Lite converted version of the same model, I get the following prompt:

CFrancesco_1-1690184772998.png

Any ideas about how to solve this problem?

 

Some information about my setup:

STM32CubeMx version: 6.8.0

X-CUBE-AI version: 8.1.0

TensorFlow version: 2.10.0

 

Thank you very much.

3 replies

Visitor II
September 5, 2023

Hi,

I have the same issue with a similar LSTM model. Did you  solve it?

fauvarque.daniel
ST Employee
October 3, 2023

The conversion to TFLite unfolds the LSTM layer in many different ways depending on the paramters of the LSTM and if it is stateless or stateful.

UNIDIRECTIONAL_SEQUENCE_LSTM is supported by X-Cube-AI, you can follow the instructions here https://www.tensorflow.org/lite/models/convert/rnn to properly convert your Keras LSTM model into a tflite model understood by X-CUBE-AI

Regards

Visitor II
April 19, 2024

Hello,

I tried the above mentioned solution but still got the same error....

I am also implementing a CRNN model which consists of CNN layers and LSTM layers inside it, but LSTM part is not being implemented. 

I am doing audio processing over the board and using LSTM can prove to be very efficient for them. 

I have X-Cube-AI 9.0.0, is there any other version I should use? Is there any other way I can work around with LSTM deployment on the board. 

My model description: 

nuvyas_0-1713517426345.png

Here, 128 corresponds to the height of the input spectrogram (frequency bins), 600 corresponds to the width (time steps or frames), and 1 corresponds to the number of channels (mono audio).

 

Any help is appreciated really,

Thanking you

N.U.Vyas