How to increase attenuation value in Teseo III RF front-end?
Hi!
UM2399 User manual ST Teseo III binary image on page 276 says:
"If a specific configuration is required (see RF front-end reference manual for details about registers) it can be achieved by setting in the proper way the configuration parameters in the range from 140 to 189."
I would like to find an information about RF front-end registers of the device (8089F) to increase RF front-end attenuation by 10 dB. We substitute 8088 by 8089 which has LNA and amplification is too hi for our input signal. I find it out by adding external attenuator - works fine CNO is 40-45. Without it works bad i think because of signal clipping.
Thank you in advance!