Teseo-liv3f (Astra1b) can't find any sattelites
Hi to everybody,
I have a annoying problem with Teseo-liv3f (on Astra1B). It can not find any sattelites. What I have:
1. Chip is build in dev kit from STM Astra1B, so there is no problem with layout, wrong antenna, etc.
2. I'm using as reference hex files from example project provided by STM: "CustomUC"
3. Kit is placed under sky, so it can see sattelites.
4. I have 3 pcs. of such kit, both can't see sattlites
5. On all devices, I program (at the beginning) my compilation of my firmware. When I realise that it can't see sattelites, I reprogram then flash by hex delivered by STM (CustomUC). Still can't see sattlites (I'm using on console command !gnssreport-on). Maybe during programming my version of firmware, I damaged some configuration bytes??
6. I though that maybe amplifier on gps antenna is off (ANToff pin13), but there is 3.3V, so seems to be OK.
7. Now, I detach on one device TX and RX of Teseo-liv3F, and I connect them (through serial / usb converter) to computer. I'm using now Teseo-Suite. I see logs, I try to reconfigure low power mode, used contellations, etc. No luck. Teseo is reconfigured, but still no sattelites.
8. I have also other gps module (Ublox Neo-7m). It works, even inside room, so this is not problem of "noisy environment".
9. I fulfill all reccomendation from this thread: STEVAL-ASTRA1B - Teseo-LIV3F GNSS Not working - STMicroelectronics Community
10. I read in Teseo-Suite Pro all info about version of Teseo. Here it is:
OS20LIB_4.3.0_ARM
GPSAPP_2.4.0.2_ARM
BINIMG_4.6.8.2_ARM
SWCFG_82045325
WAASLIB_2.20.0_ARM
STAGPSLIB_6.0.0_ARM
STA8090_822bc043
GNSSLIB_8.4.10.16.3_ARM
Maybe sombody have any clue, what I do wrong? Broken 3 devices, I doubt it. Rather I set wrong some jumpers or during programming I made some mistake.
Any clues are welcome.
Thank you in advance,
Gregor