Skip to main content
Sergei
Associate
September 27, 2018
Question

Teseo-LIV3F, no satellite position.

  • September 27, 2018
  • 15 replies
  • 9370 views

Hello, Can you help me?

I assembled a module on the Teseo-liv3f basis with a passive antenna (A25-4102920-AMT02). And I can not get the coordinates in nmea messages (screenshot in attach). What could be the problem?

Thank you.

    This topic has been closed for replies.

    15 replies

    Technical Moderator
    November 8, 2018

    Ciao Francesco, Karim

    The module in your hands isn't the final one.

    It's a prototyping sample built in ~Nov 2017.

    On board there isn't the final firmware.

    We could plan a firmware-update of the module to promote the module to the final firmware.

    @Francesco, On which board are you testing the module?

    Thanks

    Ciao

    Francesco

    FResi
    Visitor II
    November 8, 2018

    Ciao Francesco and Karim,

    The module is on a proprietary testing board. Here below the FW versions:

    OS20LIB_4.3.0_ARM

    GPSAPP_2.4.0.1_ARM

    BINIMG_4.6.8.1_ARM

    SWCFG_8204941a

    WAASLIB_2.20.0_ARM

    STAGPSLIB_5.1.0_ARM

    STA8090_622bc043

    GNSSLIB_8.4.10.16.3_ARM

    Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?

    Where can I download the bin file?

    Best regards

    Francesco

    Technical Moderator
    November 8, 2018

    Ciao Francesco

    > Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?

    if in your board you can reset the module (just with a simple push-button or similar..) yes you can.

    > Where can I download the bin file?

    We will send the binary by email.

    Is it ok?

    Thanks

    Ciao

    Francesco

    Iyaku
    Associate II
    October 7, 2019

    I can not get the activation code for Teseo-Suite Pro.

    MTzie.1
    Associate II
    July 1, 2022

    Hello

    We are having trouble to work with the TESEO-LIV3R 

    It looks like we have chips that has old firmware 

    We tried to update the FW using the Teseo-suite Pro 

    but couldnt manage to do it

    As soon as we connect to the Teseo-suite we have connection to the Com port and as soon as we try to upload the Bin file it gives us the massage that it is in Sync and it doesnt proceed from there

    Is there any other instruction then that one that is in the ST web site or if you could help me I would appricate that

    BR

    Tzif

    We have GPS modules with the 0693W00000QKIAwQAP.jpg 012 GAN80

    Technical Moderator
    July 4, 2022

    Hi

    Teseo-LIV3R is a ROM based GNSS module. You can NOT upgrade it.

    The module which support firmware upgrade are:

    • Teseo-LIV3F
    • Teseo-LIV3FL

    which are both Flash based.

    Regards

    Francesco

    MTzie.1
    Associate II
    July 4, 2022

    Thank you so much for your answer

    I have few Modules Teseo-LIV3F

    and I will try to update them

    But what can I do with the LIV3R that I bought - why cant I get the Sattelite ( I keep on getting "0" atough the layout is ok ( Tried with few antennas )

    What can I do with the LIV3R

    Please advise

    Technical Moderator
    July 4, 2022

    Please, contact Karim Ramsi (karim.ramsi@st.com)