Wake-Up Status of Teseo-LIV3F
Hi guys, i'm working with the GNSS expansion board X-NUCLEO-GNSS1A1, plugged to STM32F411RE Nucleo board. I looked inside the X-Cube GNSS1 expansion software package, which provides also some ready-to-be-built examples. I've chosen the simpler one, "GetPos", and after building and running a serial terminal, i see from the menu that the "wakeupstatus" is always "0". I've tried to add some code that set the wakeup pin, but nothing changes.
I've used the following configuration of the jumper:
J2 open
J3 closed
J4 closed
J5 open
J6 closed
J7 open
J8 open
J9 closed
J10 open
J11 open
J12 open
J13 closed
J14 closed
J15 closed
Any suggestions?