Skip to main content
RSeny
Associate II
May 24, 2019
Question

Which PPS $PSTMPPSDATA and $PSTMUTC messages related with? With previous or with next?

  • May 24, 2019
  • 1 reply
  • 1493 views

2019-05-24 10:01:31.578471543 | processPps()

2019-05-24 10:01:31.711095091 | $PSTMPPSDATA,1,1,1,0,0,0,0.500000,0,713,248,0,0,0,0,0,36,3,11,18,4,0,1.301e-08,65473955.16,25999998.74*16

2019-05-24 10:01:31.739373411 | $PSTMUTC,100135.000,24052019,1242727295,18,2*57

2019-05-24 10:01:31.739501850 | unixtime 1558692095 dUnixtime 0.000000013010 leapSec 18 leapSecValid 2

2019-05-24 10:01:32.578423766 | processPps()

Here previous PPS came at 10:01:31.578471543 local time

next at 2019-05-24 10:01:32.578423766

My understanding that quantization error from $PSTMPPSDATA 1.301e-08 should be added to next PPS signal to have precise time of the PPS. Am I right?

Following this logic $PSTMUTC should be the same next PPS second. Is this true?

Thank you in advance!

Ruslan

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    May 31, 2019

    Hi

    It seems you are using the Teseo-SDK.

    The GNSS Community is targetting GNSS Binary Image solution.

    Could you open a discussion with your relevant FAE?

    Thanks

    Regards

    Francesco

    RSeny
    RSenyAuthor
    Associate II
    May 31, 2019

    Hi, Francesco!

    I'm not using Teseo-SDK. I'm using UART to communicate with the module and digital signal 1PPS.

    So I have incoming PPS number N

    then group of NMEA messages by UART

    then next PPS number N+1

    as you can see in log in my first message with times attached.

    Seconds switched on PPS coming. My question is

    $PSTMUTC give number of a second starting from next PPS? Or this is the number of the current second started from previous to the $PSTMUTC message PPS signal?

    This is a question about how binary image generates messages and PPS signals.

    Best regards

    Ruslan

    Technical Moderator
    June 4, 2019

    Ciao

    The UTC time information reported in the  $PSTMUTC NMEA message are used to evaluates the Next PPS signal.

    The $PSTMPPSDATA reports against which UTC time the PPS has been evaluated/generated.

    Hope this helps

    Regards

    Francesco