about schematic for VL53L1X
Dear Sir,
We will make our own PCB for VL53L1X application. There are some difference between
VL53L1X breakout board schematic in UM2359 and VL53L1X schematic in the datasheet.
In Figure3 of datasheet, pin 4, 6, and 12 are connected to ground directly. But in VL53L1X breakout board, pin 4 and 12 are connected to a 1K resistor , and pin 6 is float status.
We use the connection shown in Figure3 in the datasheet of VL53L1X, I wonder if the connection is OK or not. or should we use the connection of the breakout board?
thank you very much for your help in advance.
best regards
Sai Dai