Can't Read Data from VL53L8CX using STM32
Hallo Everyone,
Here is my code:
#include "main.h"
#include "vl53l8cx_api.h"
#include "stdio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
VL53L8CX_Configuration dev; // Sensor-Konfigurationsstruktur
uint8_t status;
uint8_t isAlive = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void VL53L8CX_Initialisation();
void VL53L8CX_ReadData();
void I2C_Scan();
#define I2C_TIMEOUT 1000
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
// I2C_Scan();
//VL53L8CX_ReadData();
/* USER CODE END 2 */
dev.platform.address = VL53L8CX_DEFAULT_I2C_ADDRESS ;
status = vl53l8cx_init(&dev);
status = vl53l8cx_set_ranging_frequency_hz(&dev, 30);
status = vl53l8cx_set_resolution(&dev , VL53L8CX_RESOLUTION_8X8);
status = vl53l8cx_set_integration_time_ms(&dev, 20);
status = vl53l8cx_set_ranging_mode(&dev, VL53L8CX_RANGING_MODE_CONTINUOUS);
/*if (status != VL53L8CX_STATUS_OK) {
char buffer[100];
int len = snprintf(buffer, sizeof(buffer), "Fehler bei der Initialisierung, Fehlercode: %d\n", status);
HAL_UART_Transmit(&huart2, (uint8_t *)buffer, len, 1000);
while (1); // Stoppe das Programm bei einem Fehler
}*/
status = vl53l8cx_start_ranging(&dev);
/* status = vl53l8cx_is_alive(&dev, &isAlive);
if (status || !isAlive) {
HAL_UART_Transmit(&huart2, (uint8_t *)"VL53L8CX nicht gefunden!\n", 26, 1000);
while (1); // Wenn der Sensor nicht gefunden wird, stoppe hier
}
HAL_UART_Transmit(&huart2, (uint8_t *)"VL53L8CX gefunden!\n", 20, 1000);
*/
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
VL53L8CX_ResultsData data;
status = vl53l8cx_get_ranging_data(&dev, &data);
if (status == VL53L8CX_STATUS_OK) {
// Gib die Messwerte (z. B. Entfernung) über UART aus
char buffer[100];
int len = snprintf(buffer, sizeof(buffer), "Entfernung: %d mm\n", data.distance_mm);
HAL_UART_Transmit(&huart2, (uint8_t *)buffer, len, 1000);
} else {
HAL_UART_Transmit(&huart2, (uint8_t *)"Fehler beim Abrufen der Daten!\n", 30, 1000);
}
HAL_Delay(500); // Alle 500 ms Daten ausgeben
}
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 400000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
uint32_t errorCode = HAL_I2C_GetError(&hi2c1);
char buffer[100];
int len = snprintf(buffer, sizeof(buffer), "I2C Fehler: %lu\n", errorCode);
HAL_UART_Transmit(&huart2, (uint8_t *)buffer, len, 1000);
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
void I2C_Scan() {
uint8_t i;
uint8_t buffer[1];
for(i = 0; i < 128; i++)
{
// Versuche, auf jede I2C-Adresse zuzugreifen
if (HAL_I2C_Mem_Read(&hi2c1, (i << 1), 0, I2C_MEMADD_SIZE_8BIT, buffer, 1, 10) == HAL_OK)
{
// Gebe die Adresse aus, wenn das Gerät reagiert
char buffer[30];
int len = snprintf(buffer, sizeof(buffer), "I2C Gerät gefunden auf Adresse 0x%02X\n", i);
HAL_UART_Transmit(&huart2, (uint8_t *)buffer, len, 1000);
}
}
}
/**
* @brief USART2 Initialization Function
* None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 460800;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void c()
{
// Sensor-Kommunikation über I2C initialisieren
dev.platform.address = VL53L8CX_DEFAULT_I2C_ADDRESS;
// Überprüfen, ob der Sensor erreichbar ist
status = vl53l8cx_is_alive(&dev, &isAlive);
if (status || !isAlive) {
printf("VL53L8CX nicht gefunden!\n");
while (1); // Stoppe das Programm, falls der Sensor nicht erkannt wird
}
// Sensor initialisieren
status = vl53l8cx_init(&dev);
if (status) {
printf("Fehler bei der Initialisierung des VL53L8CX!\n");
while (1);
}
printf("VL53L8CX erfolgreich initialisiert!\n");
}
void VL53L8CX_ReadData()
{
VL53L8CX_ResultsData results; // Datenstruktur für die Messwerte
status = vl53l8cx_start_ranging(&dev); // Messung starten
if (status)
{
printf("Fehler beim Starten der Messung!\n");
return;
}
while (1) // Endlosschleife für kontinuierliche Messungen
{
uint8_t ready = 0;
status = vl53l8cx_check_data_ready(&dev, &ready);
if (!status && ready)
{
vl53l8cx_get_ranging_data(&dev, &results); // Messwerte abrufen
// Ergebnisse ausgeben (VL53L8CX hat 64 Zonen, wir nehmen Zone[0] als Beispiel)
printf("Distanz: %d mm\n", results.distance_mm[0]);
HAL_Delay(100); // 100 ms Pause zwischen den Messungen
}
}
vl53l8cx_stop_ranging(&dev); // Messung beenden
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */