Changing the cross-talk calibration distances for the VL6180X
Hello!
So in the project I am working on, we are using ToF sensors (with a cover glass) to accurately measure the distance of a white object within the ranges of 30-70mm. We would like to create a calibration fixture that also falls within these distances, but reading up on the datasheet the recommended distance to account for cross-talk is set to 100mm. Could we still get away with setting the calibration distance for cross-talk at 70mm?