Constant short reading after adding 2 mm bandpass filter – VL6180X & VL53L4CD
Hello,
we are using VL6180X and VL53L4CD sensors in an outdoor setup and we have issues with sunlight (even reflected light).
To improve sunlight rejection, we added Thorlabs bandpass filters:
FBH850-10 for VL6180X (850 nm)
FBH940-10 for VL53L4CD (940 nm)
Both filters are 2 mm thick.
The filter is placed ~1 mm in front of the sensor window.
We have four identical sensors per type; only one has the filter.
Observations:
Sensors without filter measure correctly (e.g. 143 mm → 143 mm, 70 mm → 70 mm).
The sensor with the filter almost always reports a short distance (~20–30 mm).
Even when the real target distance changes significantly, the filtered sensor reading remains almost constant.
This looks like strong optical crosstalk rather than noise.
Questions:
Is a 2 mm interference filter likely to introduce severe crosstalk?
Could the 1 mm air gap be the main cause?
Would a much thinner IR-pass filter be more appropriate?
Can the crosstalk calibration compensate for this configuration?
Any guidance on proper external filter integration for outdoor use would be greatly appreciated.
Thank you.