Detect & correct for orientation of ToF Sensors
Hello,
This is in regard to the question I posted at the webinar on AI-powered gesture recognition with Time-of-Flight sensors held on 3/11.
Can the orientation of the VL53L8CX ToF sensor be detected in case it is moved and possibly gets inverted after training is done?
I'm interested in correctly detecting gestures like LIKE/DISLIKE and SWIPE RIGHT/LEFT even if the sensor has been turned upside down after the overall device is trained. The solution should work correctly for left- and right-handed persons. It's ok to add MEMS sensors to the overall project but I prefer trying to solve problems with software first rather than just throw hardware at them, as long as the extra software doesn't bog down the MCU.
Thanks in advance and best regards,
Bruce