Does anyone have experience with measuring water / liquid levels? (Vl53L5CX)
I am currently investigating two sensors (VL53L1X and Vl53L5X) for my bachelor thesis.
In my measurements, the VL53L1X was able to achieve a measuring accuracy of 5-8 % when it is mounted exactly vertically above the water surface.
However, the VL53L5 causes me great concern. It should actually detect the water level as shown in the video on the STM site (Video: Liquid Level Monitoring using ST's Time-of-Flight: Vl53L5CX).
However, I have the problem that I don't know how to adjust the sensor. For example, if it measures with a 4x4 matrix, one of the 16 values is correct. But how can I filter this value or improve the result so that all 16 values approximately detect the liquid surface. Does anyone have any experience or tips? (Please do not use tips in the direction of float or similar, I am interested in the optimal settings of the sensor).
Currently the sensors are running on a Nucleo with the respective GUI for the expansion boards. (STSW-IMG024 and STSW-IMG008)
I would be very pleased to receive an answer.
Kind regards
Sophia