How does a VL53L0X react with multiple targets in FOV
I understand that there are models with multiple zones, but what I am trying to figure out is how a single zone TOF sensor will react when inside the FOV there are multiple targets.
For example - if there is a wall at 100cm covering the full FOV, but also an object covering say 10% of the FOV at only 50cm. What kind of measurement can be expected? What if that object covers 25% or 50% of the FOV?
Any resources that you can point me to, or a good explanation of how the measurement is made I would appreciate.
I work with FIRST Tech Challenge teams. This is for Jr. High & High School students who build robots and compete. There is a VL53L0X based sensor that is common, but there appears to be misunderstandings about how it works. I want to put together a tutorial for them, but the data sheet doesn't seem to address this situation. And this kind of situation is pretty common with how the sensor is being used.