Skip to main content
Visitor II
July 28, 2025
Solved

Image acquisition timeout with steval-evk-u0i and steval-56g3mai

  • July 28, 2025
  • 1 reply
  • 270 views

Hi Guys,

I'm on windows 11, i installed all the drivers needed (STSW-IMG501_v.1.1.1) that contains InstallCx3Driver.exe and EVK GS_1.1.1_win64.exe 

 

I have connected the steval-56g3mai module to steval-evk-u0i.

I'm trying to run the script vdx6gx_example_open_cv.py from STSW-IMG507_56G3_v.2.0.2.zip

 

What i noticed is that for some image sizes (like 600x600) the camera can acquire correctly and i see the image displayed with openCV, but if i increase the size to for example 800x800 or more i get this error from the script:

c:\tmp\windows>python vdx6gx_example_open_cv.py
Loading st_brightsense_sdk_vdx6gx.dll
IMG platform version 305 loaded :)
Boards connected: (0,P4405C-00A#0219)
No board id was specified, selecting board 0.
Initiating CCI communication at address 32
No sensor on interface 0, checking interface 1
Sensor detected on interface 1.
CSI reconfigured with 2 lanes at 1500 Mbps, 1116x1356 pixels, 8 bits per pixel, 160.8 MHz pixel clock
1119
IMG_PLAT error (1): Error: Capture timeout;(Frame not captured)
Traceback (most recent call last):
File "c:\tmp\windows\vdx6gx_example_open_cv.py", line 47, in <module>
metadata, image = sensor_dll.get_image(width)
File "c:\tmp\windows\image_sensor_python_sdk.py", line 92, in get_image
return self._frame_decode_function(self.get_raw_image(), width)
File "c:\tmp\windows\vdx6gx_frame_decoding.py", line 41, in decode_frame
bits_per_pixel = int(extract_status_line_value8(VDx6Gx_REG_STATUS_FORMAT_CTRL, raw_frame))
File "c:\tmp\windows\vdx6gx_frame_decoding.py", line 21, in extract_status_line_value8
return extract_first_status_line_value8(status_register_address, raw_frame)
File "c:\tmp\windows\vdx6gx_frame_decoding.py", line 9, in extract_first_status_line_value8
return raw_frame[register_offset]
IndexError: index 188 is out of bounds for axis 0 with size 0

 

 

This happens also if i use EVK GS software and start the component.

 

I tried to read ERROR_CODE register after issuing command start_streaming and there is no error (ERROR_CODE = 0).

 

From the board i see a green led (D8 on schematic, should mean that i'm using the raspberry connector)

Do you know how can i debug this? 

 

Thank you!

 

Best answer by Jean_Poire

Hi @SimoneGevis,

 

There might be an issue with your usb cable. Can you make sure that your cable is a usb 3.1 cable. 

Older USB C cables are only rated to 480MBits per second. That's too slow for the next generation of cameras. USB 3.1 is 5Gbits and 3.2 is 10Gbits. (see related post: Solved: My Global Shutter camera doesn't seem to work - STMicroelectronics Community)

 

Best regards,

Jean

1 reply

Jean_PoireBest answer
ST Employee
July 30, 2025

Hi @SimoneGevis,

 

There might be an issue with your usb cable. Can you make sure that your cable is a usb 3.1 cable. 

Older USB C cables are only rated to 480MBits per second. That's too slow for the next generation of cameras. USB 3.1 is 5Gbits and 3.2 is 10Gbits. (see related post: Solved: My Global Shutter camera doesn't seem to work - STMicroelectronics Community)

 

Best regards,

Jean