Limit field of view for a narrow level sensor
Hello,
I am building an IoT level sensor for a vessel. The vessel is emptied at the bottom, and I would like to sense how much stuff is still in there from the top lid. The tank is approximately 40cm deep, and 10x10cm wide and it is dark inside.
Considering the wide viewing angle of the proximity sensors (25 degrees) and the narrow vessel, I'm worried that I will get into trouble with false readings, so I was wondering if I could limit the view of the sensor, or that you might know another way of reasonably accurately (+/- 0.5cm) measure the amount of salt in the vessel.
Kind regards,
Samot