maximum temperature (while not operational) of VL53L0X ToF sensor
Hi everyone,
can you provide information on the highest temperature and ambient pressure the VL53L0X Time of Flight (ToF) ranging sensor can handle without being damaged? Note: this is not during operation of the sensor (operating temperature is given as -20 °C to 70 °C in the datasheet) but during the integration process into a larger system.
Thanks in advance and kind regards
Philip