Problem with multiple sensors (3) on the I2C bus and C++ API
Hi ST team and community !
I'm here because i have some troubles on the processus of initialisation of multiple sensors VL53L1CB.
I use the following library available on gitHub : https://github.com/stm32duino/VL53L1
The processus is the following :
- Shut down reset pin XSHUT of each sensor
Then, in a for loop (to setup my 3 sensors) :
- Power ON the first sensor with XSHUT pin
- I2C scanner to detect my only sensor ON (normally at address 0x29)
- Create my C++ component with the I2C link and XSHUT digital/analog PIN
- Init sensor with the new address with InitSensor function in the class VL53L1 of C++ API
- I2C scanner again to check if the address has been changed
Then, switch to another sensor in the for loop until initialisation of my 3 sensors.
My problem is when the for loop arrives on the third sensor, it's impossible to execute InitSensor function and the program turn to infinity.
Question is, there is a RAM probleme when i create C++ component with "new/delete" ? (load the entire VL53L1 class ?) I have 32KB of RAM
Do you have some exemple of multiple VL53L1CB (not VL53L1X) initialisation with C++ API ?
Here is my code :
const int numberOfSensor = 3;
uint8_t devAddr[3] = {0x62, 0x64, 0x66};
VL53L1 *nVL53L1[numberOfSensor];
int sensor = 0;
static const uint8_t XSHUT[3] = {0,1,2};
void setup()
{
// Initialize serial for output.
delay(5000);
SerialPort.begin(115200);
SerialPort.println("Starting...");
// Initialize I2C bus.
DEV_I2C.begin();
DEV_I2C.setClock(400000); // 400KHz
SerialPort.println("Start I2C : ok");
// XSHUT declarer en sortie et mis au niveau bas
pinMode(XSHUT[0], OUTPUT);
pinMode(XSHUT[1], OUTPUT);
pinMode(XSHUT[2], OUTPUT);
digitalWrite(XSHUT[0], LOW);
digitalWrite(XSHUT[1], LOW);
digitalWrite(XSHUT[2], LOW);
SerialPort.println("ALL XSHUT OUTPUT DOWN : ok");
// Initialize VL53L1 satellite component.
for (sensor=0; sensor<numberOfSensor; sensor++)
{
// SHUT ON reset pin of sensor
digitalWrite(XSHUT[sensor], HIGH);
SerialPort.println("XSHUT UP"+String(sensor)+" : ok");
// Search all addr connected to my SAMD21
debug_I2C_scanner();
SerialPort.println("Scanner I2C : ok");
// Create VL53L1 satellite component
nVL53L1[sensor] = new VL53L1(&DEV_I2C, XSHUT[sensor]);
SerialPort.println("Create component : ok");
status += nVL53L1[sensor]->InitSensor(devAddr[sensor]);
SerialPort.println("Statut initialisation : "+String(status));
// Search all addr connected to my SAMD21 to check
debug_I2C_scanner();
SerialPort.println("Scanner I2C check : ok");
}
}(I call the delete just after)
There is the result in the shell of the execution :
//START
Starting...
Start I2C : ok
ALL XSHUT OUTPUT DOWN : ok
XSHUT UP0 : ok
Scanning...
I2C device found at address 0x19 !
I2C device found at address 0x1E !
I2C device found at address 0x29 !
done
Scanner I2C : ok
Create component : ok
Statut Initialisation : 0
Scanning...
I2C device found at address 0x19 !
I2C device found at address 0x1E !
I2C device found at address 0x31 !
done
Scanner I2C check : ok
XSHUT UP1 : ok
Scanning...
I2C device found at address 0x19 !
I2C device found at address 0x1E !
I2C device found at address 0x29 ! // NEW SENSOR ON
I2C device found at address 0x31 !
done
Scanner I2C : ok
Create component : ok
Statut Initialisation : 0
Scanning...
I2C device found at address 0x19 !
I2C device found at address 0x1E !
I2C device found at address 0x31 !
I2C device found at address 0x32 !
done
Scanner I2C check : ok
XSHUT UP2 : ok
Scanning...
I2C device found at address 0x19 !
I2C device found at address 0x1E !
I2C device found at address 0x29 ! //NEW SENSOR ON
I2C device found at address 0x31 !
I2C device found at address 0x32 !
done
Scanner I2C : ok
//STOPI need help ! I don't understand...
If there any C++ dev in the community, don't hesit to tell me what's my error.
Best regards,
LM