Ranging results values for VL53L4CD
Hi,
I am getting started with VL53L4CD so as to improve our system under ambient daylight conditions, which is performing poorly due to current sensor VL6180x under such condditions.
My application is:
- Waking up device when target detected closer than 130 mm or so.
- There is a fixed flat target at 150mm (part of the housing itself). Device is calibrated so as to avoid waking up when ranging at this this distance.
- No need to high acuracy.
I have found some range results that are not documented in API (values 7 and 255):
DEBUG LIMITS [MP: 5] [Signal min: 1496] [Sigma max: 45] [ROI with: 4]
-DEBUG-: [ 32,911 s] DATA: Status = 7, Estimated distance = 396 mm, Signal = 13080 kcps, AmbSignal = 3888 kcps, Sigma = 26 mm
-DEBUG-: [ 32,917 s] RANGE KO
-DEBUG-: [ 32,921 s] [L1] : No detect !I am using UltraLow power driver [en.STSW-IMG034].
I have tested in ambient light conditions and found some troubles comapred to indoor results.
I would like to know if there are specific settings for ambient daylight conditions? If so, could you share it so I can test them?
Regards, Ramón.