"Static object Removal" concept possible on latest VL5xx sensors?
ST,
Another non-IR sensor we have worked with has something called 'static object removal' in its microcode.
When this function is turned on for a given range, it internally histograms the environment so that objects within this range 'get deleted from consideration' after a few seconds- this allows intruders which subsequently enter within this zone to then be detected. Happily, human intruders (elbow tip, hand etc) are not stable enough or of consistent surface regularity/ reflectance to - even if slow & not moving - get 'deleted', so intrusion detection is not lost even though a fixed object left 'in view' will get 'deleted' after a few seconds.
Is there anything like this on the latest ST VL5xxx sensors or would this require substantive external processing?
Bill Wiese
San Jose CA
bill@bwiese.org